6/22/2019 5:40 AM | |
Posts: 2 Rating:
|
i want to download the parameters from drive to pc but having error.
Attachment1.pdf (330 Downloads) |
6/24/2019 4:24 PM | |
Joined: 9/27/2006 Last visit: 9/4/2025 Posts: 12397 Rating:
|
Hello M usm; Information is always helpful if you want to ask for our help. Which version of Starter are you using (we only know you are using Starter because of the hints on the screenshots you sent).? What Windows OS do you have installed on your programming PC? What model of MM4 drive are you using? Could you please verify your installation for exchanges between Starter and your drive, for example based on the following document? STARTER: How should I set up a point to point communication connection between a PG/PC with STARTER and a MICROMASTER 4 (MM4)? https://support.industry.siemens.com/cs/ww/en/view/20016155 Hope this helps, Daniel Chartier |
6/25/2019 11:45 PM | |
Posts: 2 Rating:
|
Dear Daniel Chartier , thanks for help me now i am attached some information about our system. i can go online with this kit and also upload the parameters successfully but when i download DRIVE to PC its having the error same before i send you in last mail. Attachmentdata.pdf (325 Downloads) |
Follow us on