4/2/2024 11:25 AM | |
Joined: 1/9/2019 Last visit: 3/22/2025 Posts: 88 Rating:
|
Hi experts. I have a problem and glad if you can help me on it. I have a system controlled by BECKHOFF TWINCAT V2.9 running on windows NT. in this system there is 7 motion control Axis. the drives are BECKHOFF AX2000 MOTION CONTROL DRIVES communicating IPC with Light Bus (FC200x) and the distributed module are also communicated with Light Bus. All of my servo motors are SEW, but if needed I can change them to siemens servo's As you surely know, the AX2000 drives are out of production for some years, So I wanted to replace them with SINAMICS S120 double motor modules controlled by CU320-2DP ,with communicating protocol of Profi-Bus (I can add Profi-Bus card FC3102) is it possible? if its possible is there any manual for how I can do that? AS I see in system manager of TWINCAT 2.9 there is ProfiDrive MC 'S (picture 1) (as I saw before in other projects, these ProfiDrives used for SIMODRIVE U , can I use them here for Sinamics S120 ??). ------------------------------------------------------------------------------------------ |
Last edited by: mpakravanan at: 04/02/2024 11:27:03Last edited by: The Helping Hand at: 04/02/2024 13:29:48New subject after splitting |
|
4/3/2024 3:18 AM | |
Joined: 10/17/2007 Last visit: 9/8/2025 Posts: 4442 Rating:
|
Dear mpakravanan in Siemens forum, we DO NOT discuss 3rd party HW or SW. I suggest you contact you local Siemens sales team inform them your request they will give your solution and order list. Then they will suggest you how to get "turn key project" If you want to DIY , you need ask them to have basic training one simple idea in SINAMICS S120 you need a control unit call CU320 AND THE SW for Set up call "Starter" (NOT SIMO COM U) Hope my answer help you. mpakravanan
|
If you like my comments please |
|
This contribution was helpful to
1 thankful Users |
Follow us on