2/20/2013 12:15 PM | |
Joined: 5/13/2012 Last visit: 9/14/2024 Posts: 179 Rating:
|
thank you very much mike for answer first of all 1-client request us to use siprotec device and BCU from siemens because he want to extend his substation . 2-the exsit vendor is ingteam company using PROCOME protocol between UCS(substaion control unite) it is collect data from BCU(TCP-m) and protection devices and then dend it to Control center and HMI . 3-i must give him an answer with yes we can connect siemens device support this type of protocol or not ? 4-i have read in the manul Ingteam product that if you need to connect device support IEC61850 you should contact us. what should i do? thank you very much to support me Attachment15PG-00-BBY-EMP-IGT-004 Rev 0 - UCS_IH_Info.pdf (396 Downloads) |
best regards |
|
Follow us on