11/27/2024 6:04 AM | |
Joined: 3/14/2008 Last visit: 9/3/2025 Posts: 2216 Rating:
|
Hi, This can mean two things I believe: 1. It is a HART module and the hart modules are not inserted. See FAQ: Link 2. You are using a module which is not released for PCS7 V9.1. Please check the Released modules manual: Link |
If I could help you, you can use the RATE button. Thank you. |
|
11/28/2024 5:10 AM | |
Joined: 1/11/2019 Last visit: 8/14/2025 Posts: 899 Rating:
|
Hello nill.961. Confirm Module Compatibility
2. Check and Update Module ConfigurationFor Analog Input (AI) and Analog Output (AO) modules:
|
11/28/2024 11:28 AM | |
Joined: 11/10/2022 Last visit: 5/23/2025 Posts: 23 Rating:
|
Hi Techno_Taru Need to update PCS7. This was the link which helped me. Need to download UC06 files and to follow instructions listed in Sl No 3. SIMATIC PCS 7 V9.1 SP2 Software Updates - ID: 109812242 - Industry Support Siemens Regards Nil |
Last edited by: nill.96 at: 11/29/2024 02:11:49 |
|
This contribution was helpful to
1 thankful Users |
Follow us on