10/25/2024 2:02 PM | |
Joined: 2/1/2010 Last visit: 9/9/2025 Posts: 212 Rating:
|
Correct is often a matter of opinion. The CMT's given by Siemens in the BCM are a good starting point for further customization according to your specific needs. Control Module (CM) Technology - Efficient Engineering with SIMATIC PCS 7 Regarding SFC commands, I think most experts will agree with me that you should lean toward SFC Type, not SFC. In either case you should be writing the PID to SP_Ext and putting it in external mode via SP_ExtLi when writing. If you're using the CMTs and SFC Types with, you can use the commands and statuses provided by CMT instead of addressing the nubs directly. |
If my post helped you, please rate. Thanks. |
|
This contribution was helpful to
1 thankful Users |
Follow us on