7/25/2020 9:27 PM | |
Joined: 3/30/2020 Last visit: 9/15/2025 Posts: 5451 Rating:
|
This may be helpful.. [ TIA Selection Tool ] |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
7/27/2020 2:07 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi Nitish_Patil, S7-300 and S7-400 Controller are an older genereation of Siemens Controller, which are still on the market. The S7-1500 and S7-1200 controller are the new generation controller. You can find an overview for the new controller in the S7-1500 system manual, chapter 3. SIMATIC S7-1500, ET 200MP Automation systemAs you can see in the oveview and the performance of the different controller it is not only depending on the amount of Input which controller should be used.(have a look on the complete chapter 3). hope this helps, regards |
FCK WAR! |
|
7/27/2020 3:02 PM | |
Posts: 31 Rating:
|
Thank you for the answer! I will look into it.
I am looking at the Desigo PXC. I can see that is has loads of analog and digital input and I can add more as it's modular. Can I write logic like a standard PLC in it? Sorry if I come out as a newbie, that's because I am. |
7/29/2020 9:46 AM | |
Joined: 7/25/2012 Last visit: 8/20/2025 Posts: 291 Rating:
|
Yes, Desigo PLC's are free-programmable controllers. Environment is tool with the name XWP (Xworks Plus) and programming tool is CFC, which we have licensed separately from original. It is same tool as for S7, but under different license. Desigo products are developed for building control, so if you need PLC for an industrial case/project, then S7-1500 will be the right product. For XWP you have to buy 1-years license and be a solution partner for Siemens SI BP. Contact you local Siemens office for more detailed info about how to be Solution Partner. Or let me know via personal message from where you are, and I can try to find an office. |
Best regards, |
|
Follow us on