8/28/2009 2:43 PM | |
Joined: 5/28/2008 Last visit: 9/1/2025 Posts: 901 Rating:
|
Hello IvanG, I think your problem is quiet easy...i can´t believe that it is a bug of protool In my opinion the problem is your programm for the CPU...maybe you reset the bit after setting the bit? please have a look to your s7 programm.... regards manfred |
8/28/2009 3:30 PM | |
Joined: 5/28/2008 Last visit: 9/1/2025 Posts: 901 Rating:
|
did you realy choose a switch? could you post some screenshot or the project? |
8/31/2009 12:30 PM | |
Posts: 6 Rating:
|
Here is a screenshot of the Step 7 and Protool program. All I want is that when I set input "Ulaz 1" (I 0.0), I set the output "Izlaz" (Q 0.1). I have the simulation module SM 374, and it works OK. But, when I start Protool runtime mode and put the switch to ON position (switch is connected to tag "Ulaz 1"), it resets and returns to the OFF position at the end of every cycle. If you have any ideas, I would appreciate it. AttachmentScreenshot.pdf (422 Downloads) |
8/31/2009 2:09 PM | |
Posts: 6 Rating:
|
Thank you all.... It works now :) |
This contribution was helpful to
1 thankful Users |
Follow us on