7/3/2010 6:02 PM | |
Posts: 8 Rating:
|
Hi ! Iam facing a problem with Simoreg Dc spindle drive 6RA2677.. series D380/250 The moment we enable the drive and give speed comand , the field fuse is blowing . Which will cut off the supply to the drive electronics . Now if I remove one of the Armature connection to the motor and switch on the drive enable. The drive stays on and the field also gets on . We get the field voltage of about 400Volts. The Field resistance is about 69 Ohms. Can any body share their Ideas. With Regards: Shiva Splitted from siemoreg. |
Last edited by: O_Moderator at: 7/5/2010 8:18 AMnew subject after splitting |
|
Follow us on