2/13/2023 2:16 PM | |
Posts: 4 Rating:
|
Yes, all my image boot tries get stuck; only boot the internal eMMc with pre-installed IndOS. |
2/15/2023 2:47 PM | |
Posts: 4 Rating:
|
Sure, here you go Attachmentboot sequence.txt (568 Downloads) |
2/15/2023 3:47 PM | |
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi, you are able to boot from the Industrial OS right? Can you try to update the firmware using the Industrial OS? I am not 100% whether it works, but it is worth a try. - Download and extrace the attached .zip file - Copy both files to your IndOS - Install firmware update tool:
- Update firmware:
Then try to boot Example Image V1.2.2. If you have problems during this process, I am happy to help. Best regards! Attachmentfirmware_update.zip (729 Downloads) |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
6/12/2023 1:43 AM | |
Joined: 4/6/2021 Last visit: 8/26/2025 Posts: 6 Rating:
|
Hi, I'm getting the same issues. Did you manage to resolve this? I have 2 devices, and both are doing the same thing. |
7/5/2023 8:41 AM | |
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi, you can use the Example Image V1.0.2 to update the firmware: IOT2050 Bricked? - 297151 - Industry Support Siemens Another try could be to add the line BUILD_ID="V01.01.01" to /etc/os-release to your IndOS and try the update again. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on