3/16/2019 8:03 AM | |
Posts: 9 Rating:
|
Dear Sir Hi, Thanks for your information. I have some questions in regard of cement batching plant if you can help us. For weighting system we use 4 load cell transducers with Modbus RTU output to connect them to s7-1200. Is it possible? I mean is it accurate and fast enough for reading weight? For aggregate gates we use pneumatic air cylinder to open or close them? i wanted to know is that all that we have to do to control the weight? to have an approximate weight with max 10 kg error? or should we design a PID loop in PLC to close the gate? Thanks in advance for your time ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/18/2019 7:43:22 AMNew subject after splitting |
|
3/20/2019 4:41 PM | |
Joined: 1/4/2007 Last visit: 8/26/2025 Posts: 1190 Rating:
|
Hello ACM-1899, For a dosing application in S7-1200, normally the Siwarex WP251 module is used. Best regards Siwarexi AttachmentFlyer_SIWAREX WP251_EN.pdf (377 Downloads) |
Follow us on