11/7/2024 10:16 AM | |
Joined: 5/6/2022 Last visit: 9/9/2025 Posts: 589 Rating:
|
Hi SaverH, In this case, it would be helpful if you could comment on the following information: 1- If you load another basic project and try to simulate it does the same thing happen to you? 2- What software are you using exactly (version, etc)? 3- Are you working with a virtual machine? 4- Windows version screenshot. Windows + R, type "winver" in the box, open and then select OK. 5- Please check again in which status a project is in Runtime Manager after trying to start it. If the project is "Partly Running", please check the following: Does the user currently logged in Runtime have sufficient rights? Is the user registered in the following Windows user groups: - PlcSimUsers - RTIL Tracing Users - Siemens TIA Engineer - SIMATIC HMI - SIMATIC HMI VIEWER 6- Is the device name no longer than 15 characters? Is "OPC UA" enabled in the Runtime configuration and is a certificate available? Best regards!
|
If this Information really helps, you could use the Rate function |
|
11/8/2024 12:06 PM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello SaverH does it appear with any project? also with a new one? Make your certificates new and check if you have set up everything properly: https://support.industry.siemens.com/cs/de/en/view/109806850 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on