6/12/2025 1:17 AM | |
Joined: 7/7/2015 Last visit: 9/2/2025 Posts: 58 Rating:
|
Dear all. I have questions for the setting of Scalance. There are several Scalances, it has red ramp. And sometimes the communication alarm occurs radomly. So I check the diagnostic on Scalance and it says, 'Non-recoverable error: More than none RM in ring' But the net woks system is not 'Ring' and i want to disable this funcion. My question, 1. Is the initial setting of 'Redundancy Type', 'Ring'? 2. Could 'Non-recoverable error: More than none RM in ring' error affect to communication condition? Thank in advanced! AttachmentSCALANCE.zip (106 Downloads) |
6/24/2025 9:39 AM | |
Joined: 8/3/2009 Last visit: 9/16/2025 Posts: 16412 Rating:
|
In the manual there are a few information about the factory settings: https://support.industry.siemens.com/cs/ww/en/view/109988863/173152725771 perhaps this helps Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on