3/22/2016 12:00 PM | |
Joined: 3/3/2006 Last visit: 3/20/2025 Posts: 30 Rating:
|
Hello all I have an item about Simadyn D and ET200SP. I like to change ET200M to ET200SP. I have configured one 16 bit input module and one 16-bit output module. Configuration works fine in ET200M. Then I change configuration (COM Profibus ver 5.2) and when I download new configuration to SS52 board, there come fault C to CPU (PM6). Also SS52 board is blinking 1 hz, which means in manual that COM database not exist or not activated. Fault code 6074 says that check parameters on CTV block. But is there any parameter modification needed becouse station number and number of IO's remain same?
Jari AttachmentSimadyn D and ET200SP.pdf (426 Downloads) |
Last edited by: puurtja at: 3/22/2016 12:04:54 PMLast edited by: puurtja at: 3/22/2016 12:20:39 PM |
|
3/22/2016 12:22 PM | |
Joined: 8/25/2006 Last visit: 9/15/2025 Posts: 2218 Rating:
|
Hello. Did you delete old station ET200M and configure new station ET200SP in ComProfibus with the same DP-address and same length of I/O's? GSD-files of ET200SP for integration in ComProfibus you can find here. |
3/23/2016 6:55 AM | |
Joined: 8/25/2006 Last visit: 9/15/2025 Posts: 2218 Rating:
|
Hello. Did you fill I/O's addresses as shown on my screenshot? |
3/23/2016 11:53 AM | |
Joined: 3/3/2006 Last visit: 3/20/2025 Posts: 30 Rating:
|
Hello Yes I restart Simadyn D. Here are projects. Struc is made version 4.2.5. Jari AttachmentCOM and STRUC ET200SP.zip (326 Downloads) |
3/23/2016 7:10 PM | |
Joined: 8/25/2006 Last visit: 9/15/2025 Posts: 2218 Rating:
|
Hello. I could not find anything wrong in your projects. What are the values at outputs of @CSL2A? What is the exact version of ComProfibus do you have? Did you try to download with this version of ComProfibus previous configuration with ET200M after loading configuration with ET200SP and this worked fine? Once, I saw the problem with incorrect installation of ComProfibus (in that case database didn't loaded completely). Did you try to reinstall ComProfibus? Latest SP ahd HF you can find here. |
Follow us on