1/25/2024 12:49 PM | |
Joined: 12/16/2009 Last visit: 1/26/2024 Posts: 5 Rating:
|
Dear all ! I have the following problem: I have two IOT2050 Advanced FS3, one has the IndustrialOS V2.1.1 installed on the eMMC (which is booting fine, unfortunately no one knows the password anymore....) And one with apparently erased eMMC, also FS3. (Both were purchased at the same time). The problem is I can't upgrade to the new firmware, because the supplied image V1.1 when booting from mmc0 will initially load the kernel but at some point it will fail with an error. (Issue is on both IOTs). So I tried the current example image, it boots without problem, but all peripherals are not working properly, including access to SPI flash memory, so the trick described by one user to just change the version in the os-release file to trick the system to perform the fw-update, won't work. Booting the current service stick also fails (yes I know the firmware requirements are not matched (causes a reboot on both devices), but it was worth a try. So my question, where do I get a proper ServiceStick image or a working example image, so I can upgrade the firmware in order to use the current releases ? Or can I set boot options on the V1.1 image to perhaps overcome the error Issue. Here is the output of the V1.1 boot process: [snip] Thank you in advance for any help, Martin AttachmentBoot Process.txt (321 Downloads) |
Last edited by: The Helping Hand at: 01/25/2024 13:51:59Boot-Process-Log added as txt-file |
|
1/26/2024 7:58 AM | |
Joined: 6/27/2017 Last visit: 6/26/2024 Posts: 158 Rating:
|
An now your issue is solved? |
Follow us on