8/9/2006 9:43 PM | |
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hi Jef, For installing the software you need Administrator rights, after the install you don't need that rights any more. For installing the STEP7 V5.2 SP1 software you need the rights that are described in the next link: Which user rights do you need to work with STEP 7 versions V5.2 and V5.3 in MS Windows NT/2000/2003/XP? For the Access rights you can read the next link: How can you assign Full Control access to the STEP 7 installation directory? I have Windows XP Professional SP2 with STEP7 V5.4 and don't need Administrator rights. Which version do you have?
|
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
8/10/2006 6:54 PM | |
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
[quote user="Hodaka"]Well, although all of the directions says that version 5.2 should work with setting full access on the program directory, tech support tells me that non-admin accounts will only work with version 5.3 sp3 and above. This is contrary to all of the FAQs links that Late and I both posted.. I guess we're out of luck then.. I hope someone updates those FAQs with correct information, because I spent a huge amount of time trying to get v5.2 sp1 to run.. Hi Jef, Thats life, but I agree with you that it is not good written in the FAQs and Manuals. [:(] Maybe it is better to upgrade to STEP7 V5.4 so that everything is working well with the rights [:blush:] You can upgrade to STEP7 V5.4 by a upgradepackage: STEP 7 V5.4 Released for Delivery If you have the standard STEP7 (no Professional) then you need the number 6ES7810-4CC08-0YE5 SIMATIC S7, STEP7 V5.4 UPGRADE FOR ABOUT 400€ |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on