7/13/2017 7:10 AM | |
Joined: 6/29/2017 Last visit: 7/24/2025 Posts: 7 Rating:
|
Dear nulizhang: our machine had run a few years,the control system comprise Simodrive 611U &some POSMOA drive, S7-315-2DP PLC Profibus control .The Simodive 611U Double Axis control Conveyor belt, A Axis maser, B Axis slave.the other single Axis control bridge move ,open -close ; The problem sudden happen no other faulty message on OP .or 611U display unit.,NO do anything , wait a moment( or serval minutes or hours),then autorun , I am not stay at machine side ,let my colleague check some par with 611U operation unit .see attachment. My question , IR/NE controller enable signal T64 Status through Equipment Bus to transfer to other Axis,why single Axis T64 Signal ok,but double Axis T64 Signal Off. I had replace double control card,the problem occur one time,then replace NE module ,the problem No occur five days. Thanks a lot; Attachmentsimodrive611 u not run1.pdf (414 Downloads) |
Follow us on