6/3/2016 11:33 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Please refer FD 8513 (Is attached here with for ready reference), control word 1 bit 2 is for OFF3. It is controlled via P558. This is operated by CB data word 1 bit 2 i.e. B3102. So need to check this if it is 0 it means quick stop command is applied to drive. You need to connect drive monitor to check the status of Control word 1 or can check on PMU at r550. HTH. AttachmentMasterdrive MC OFF3 .pdf (594 Downloads) |
8/19/2016 12:41 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4759 Rating:
|
New question published by Mohit Kumat is split to a separate thread with the subject Simovert MC, fault history parameter. Best regards |
Follow us on