7/23/2009 8:55 AM | |
Posts: 9 Rating:
|
Dear Diwa, I have encountered 1 customer having the above problem. The CU2 is connecting to a SCB board as well. When the motor stops,after some times, the drive will start by itself without having any ON signal. When i monitor using DriveMonitor, I noticed thatbit 0on control word 1is OFF.The motor is running at 10Hz during the automatic restart. This situation happens spontaneously.How is this possible? Please find the attach parameter list Thanks a lot AttachmentSeparator100709.zip (308 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on