2/22/2012 10:36 AM | |
Posts: 27 Rating:
|
Thank you Mr Mata. In a standard application, the current maintained is to supply for exciter coil and the voltage denpends on the reristance. but in my system, DCM is used to supply to 5 parallel exciter units which are not distributed DC current evently. The current system uses a DC generator - 115VDC, 12kW,105A- to supply for those 5 exciter coils. And in my view, the DC generator is a voltage souce while with a specified current setpoint, a DCM is a current source, and there is nothing to ensure that the currents flow into sub-circuit according to the existing desin. So could you give me an advice to solve that problem.
Attachmentdcm.zip (587 Downloads) |
Follow us on