1/12/2024 8:41 AM | |
Joined: 9/23/2005 Last visit: 9/1/2025 Posts: 5111 Rating:
|
Do you have mentioned motors available ? They are phase out products and can't be bought from Siemens anymore. To connect motors to drives you only need matching cables. But to make any use of your setup you require some DC link supply (BLM/SLM/ALM) and a control unit (e.g. CU320-2PN) + CF card with licences. To make your life easier you may wish to use a technology CPU, eg. S7-1505D would match perfectly. Then CU320 is not required. For this setup without CPU you can use Sinamics Startdrive. With a T-CPU additionally TIA Step7 is required. Using TIA Selection Tool to configure your HW setup can be helpful. |
Regards, |
|
This contribution was helpful to
1 thankful Users |
1/12/2024 9:03 AM | |
Joined: 2/10/2016 Last visit: 3/27/2025 Posts: 118 Rating:
|
Hello Jack Thanks alot for your reply. I don't have these motors, so I will use 1FT7 instead. Is it available? |
1/12/2024 9:16 AM | |
Joined: 9/23/2005 Last visit: 9/1/2025 Posts: 5111 Rating:
|
Using TIA Selection Tool would give you only available parts. Or get current catalogue. Otherwise once you selected a motor you can confirm its availability at the Industry Mall. |
Regards, |
|
Follow us on