1/26/2023 5:04 AM | |
Joined: 9/23/2011 Last visit: 8/26/2025 Posts: 45 Rating:
|
Hi to all, to using it without plc, on which parameters do i need to write speed and enabling? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/26/2023 11:06:52New subject after splitting |
|
1/26/2023 2:48 PM | |
Joined: 7/7/2010 Last visit: 9/5/2025 Posts: 16061 Rating:
|
Install an appropriate advanced operator panel (AOP) into the Sinamics drive Control Unit. Now you have local drive control without a PLC. You can also use an extension kit to relocate the AOP further away from the CU, like on the enclosure cabinet or door containing the VFD. If you need more control, you can wire up a speed input and switches / buttons according to each drive's requirements. As already stated, refer to the manual for each drive on how to perform those tasks. If you need more generic information, contact your local Siemens sales rep or distributor for assistance selecting the right VFD for your specific needs.
|
science guy |
|
Follow us on