3/19/2013 9:47 PM | |
Posts: 51 Rating:
|
Is there no one that know anything of this?? Or maybe there are too many sub-forums and no one is looking here...
|
3/20/2013 9:57 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello Pontus, About transferering a project using routing, I found the following link: how do you use WinCC flexible to transfer a project to an operator panel via S7 routing? Unfortunately it is only about WinCC flexible. Your second question: You can simulate your panel on a PC. When this PC is connected to the PLC, you will have to use the right PG/PC interface. (you have to use an unique address, because the HMI use the same address) Best regards, Wizard |
Follow us on