1/5/2009 9:00 AM | |
Posts: 14 Rating:
|
can someone here can tell me how to set masterdrives to start and stop 2 different places. 1 is from PLC and 1 is from field. which parameter to set? thanks |
1/5/2009 3:45 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello Cipuden, Let's start with standart way: Your PLC is connected to the drive via profibus. Easier because here has example. Other way: Use 2 stop and 2 start buttons connected in paralel connected directly to Digital Input. And in drive parameters must assign P554 to B0010. More see in manual (page 511). In this case using a PLC is not necessery. Just the systems goes more expensive. regards |
Last edited by: UMENCHO at: 1/5/2009 5:00 PM |
|
Follow us on