6/20/2024 11:03 AM | |
Joined: 5/6/2022 Last visit: 9/9/2025 Posts: 589 Rating:
|
Hi Madadi, Looking at the compatibility tool https://support.industry.siemens.com/cs/ww/en/view/64847781 you must have at least Step 7 V5.7 Upd2 and at least Update 7 of WinCC 7.5 Sp2 installed You should also note the following: In order to use STEP 7 in integrated mode, the S7-PM Project Messages V5.7 package must be installed and licensed as of STEP 7 V5.7. Best regards! |
Last edited by: The Helping Hand at: 06/20/2024 11:35:37Text formatting optimized Last edited by: The Helping Hand at: 06/20/2024 11:35:56If this Information really helps, you could use the Rate function |
|
Follow us on