7/21/2011 6:19 AM | |
Posts: 62 Rating:
|
I search best solution for following object Logo! v5, means motor e.g. "Schischeck" or "Bellimo" ( pre-defined in 5% via PID-control Jumo) with forced opening and closing for damper, valve or jalousie. 2 Sensors. 1 Sensor- position 0% 2 Sensor- position 40%, somewher, it recks not. test 1. Step drive run to Sensor N1, position 0% 2. Step nextly, after actuation of Sensor N1 run to Sensor 2. 3. Step In closing afteractuation of Sensor N2 B002 generate signal "Test O.K." oll run apart from situation when Test begin by active Sensor N1... I have one idea, befor Test force shor Impuls OPEN. But it me displease. Attachmenttestdrive.zip (571 Downloads) |
Last edited by: Oll Bell at: 7/21/2011 6:19 AM |
|
Follow us on