11/19/2024 6:27 AM | |
Joined: 5/25/2024 Last visit: 9/2/2025 Posts: 38 Rating:
|
Hi, What's the meaning of valve with black strips? I can't seem to find the manual for this... |
11/19/2024 6:54 AM | |
Joined: 3/14/2008 Last visit: 9/1/2025 Posts: 2215 Rating:
|
Hi, The two icons on the left side (number 1 and 2) are rotating block icons. If they are opened, they will change from horizontal to vertical (icon 1) or vertical to horizontal (icon 2). The two icons with the black stripes are non rotating icons. The rotating icons are created for color blind people so that can actually see if the valve is opened/closed regardless of the color. We tend to use the non rotating icons because it looks a bit stupid, but it's perfect for color blind people. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
Follow us on