10/17/2024 8:29 PM | |
Joined: 4/28/2015 Last visit: 8/29/2025 Posts: 20 Rating:
|
I am having the same issue. When I go to the table view screen, the table view window has an overlay of the previous screen. Then I set the table view screen as the startup screen and got a blank table. When I opened the same project on a different computer, all of the table view objects displayed correctly. WinCC RT Pro v14 SP1 : Windows 11 w/ 16GB RAM and 4GB Video <-- does not display properly. Windows 10 w/64GB RAM and 6GB Video <-- displays properly. I can not say the problem is a Windows 11 issue; only that there is something different about the two computers as the video properties are similar and the video memory usage is very low on both. I did find that there was a different virtual memory size and I increased the Windows 11 machine to the "recommended" paging file size but that did not solve the issue. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 10/18/2024 06:38:19New subject after splitting Brian T Kinard |
|
10/24/2024 7:23 AM | |
Joined: 8/3/2009 Last visit: 9/11/2025 Posts: 16400 Rating:
|
Hello WinCC Professional Runtime V14 Sp1 is not released for Win11 Please check the compbatibility lists: https://support.industry.siemens.com/cs/de/en/view/64847781 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on