6/29/2022 3:31 PM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Hello noyacbr, |
With best regards, |
|
This contribution was helpful to1 thankful Users |
6/29/2022 8:28 PM | |
Joined: 12/6/2016 Last visit: 5/9/2024 Posts: 81 Rating: (3) |
hi friend, Yes you are right, we have several types of cu. This is CU240E-2DP with DI4, DI5 for SAFETY FUNCTIONS. I've been reading about your link and i confused.. i've severa pdf about this. 1. after release the sto the drive is ready SAFETY ready after release sto its ready 2. i need a f-di for ack, then this cu not right because have only two f-di (used for the channels of relay) SAFETY ack with f-DI When you say "start the drive again" you say P840? AttachmentDesktop.zip (224 Downloads) |
Last edited by: Jen_Moderator at: 06/30/2022 09:45:49Links removed and files added as an attachment. |
|
6/30/2022 5:59 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Yes. |
6/30/2022 8:41 AM | |
Joined: 12/6/2016 Last visit: 5/9/2024 Posts: 81 Rating: (3) |
Sorry AttachmentDesktop.zip (242 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on