5/30/2024 6:05 AM | |
Joined: 11/24/2022 Last visit: 9/1/2024 Posts: 6 Rating: (0) |
|
6/14/2024 1:36 PM | |
Joined: 11/24/2022 Last visit: 9/1/2024 Posts: 6 Rating: (0) |
Thanks for your answer I added INIM Fire alarm user manual. U can find Description about Modbus in it. Whole of the PLC Programming is just the Modbus client function. the project is just for communication with Fire Alarm set. I changed the "REQ" input to combination with " Done " & "Error ". As you can see in the screen shots of online program, the status of the function is "7006 " and "BUSY" is ON. As you can see in "modbus4" screen shot, "Done" isn't set so the data isn't completely received. Thank you. AttachmentModbus.zip (178 Downloads) |
6/17/2024 9:45 AM | |
Joined: 11/24/2022 Last visit: 9/1/2024 Posts: 6 Rating: (0) |
Dear qwazee can you help me I sent screen shots of online program. thanks |
6/20/2024 10:27 AM | |
Joined: 11/24/2022 Last visit: 9/1/2024 Posts: 6 Rating: (0) |
Dear sirs Can anyone help me to solve the problem ? |
Follow us on