9/24/2010 11:32 AM | |
Joined: 8/30/2010 Last visit: 9/4/2025 Posts: 31 Rating:
|
Hello Bell, Thanks for your support. [schnippschnapp] One more thing I want to tell you that I am reading values from MAG8000 device on Modbus RTU protocol. The refresh rate of device values are very fast. I can see changing values in PLC Status chart but in winCC its not changing at all. May be because it takes almost 1.2 second to send data to wincc through sinaut micro sc server (Min 1 second for Sinaut micro sc Server by value update+250ms for wincc). To solve this problem Shall I move values to another variable after two second to send to WinCC? OR Is there any alternative solution? Waiting for your reply. Thanks and Regards, Jeetendra Splitted from GPRS connection using MD720-3. |
Last edited by: O_Moderator at: 9/28/2010 10:14 AMLast edited by: O_Moderator at: 9/28/2010 10:12 AMnew subject after splitting |
|
Follow us on