(0)| 3/17/2013 12:38 PM | |
|
Joined: 6/29/2011 Last visit: 12/20/2025 Posts: 128 Rating:
|
how to communicate wincc explorer and s7-200 cpu 226 |
|
PARANTHAMAN |
|
| 3/17/2013 12:47 PM | |
|
Joined: 11/8/2011 Last visit: 1/14/2026 Posts: 387 Rating:
|
Hi paranthaman WinCC You can't use WinCC together with S7-200 in the easy way. There is no communication channel especialy for S7-200. But there isone soulution to use S7-200 and WinCC together. Use the PC-Access OPC-Server (for S7-200)and the WinCC OPC communication channel. You need: - PC-Access (max. 8 Connections); [https://www.automation.siemens.com/_en/s7-200/Products/03Software/pcaccess.html] - RS232 or USB /PPI-Cable [https://www.automation.siemens.com/_en/s7-200/Products/05Zubehoer/index.html] and also see here it has been discussed here FAQ |
Last edited by: Saggy at: 3/17/2013 12:48 PM |
|
This contribution was helpful to
|
|
| 3/17/2013 1:14 PM | ||||
|
Joined: 9/27/2006 Last visit: 1/20/2026 Posts: 12481 Rating:
|
Hello paranthaman; If you are looking for ways to connect a S7-200 CPU to WinCC, first look up this (older) FAQ: What are the options for accessing an S7-200 with WinCC? Some of the addresses in theFAQ above might not be current, so here are some updated links: PC-ACCESS OPC server for S7-200` Allmendinger link (modified): http://www.allmendinger.de/Produkte/WinCCKommunikation/MODBUSProtocolsChannelforWinCC/tabid/1874/language/en-US/Default.aspx |
|||
This contribution was helpful to
|
||||
| 8/3/2013 7:50 AM | |
|
Posts: 144 Rating:
|
hi with an EM277 module u can do it via Profiibus as mentioned below "Communication via PROFIBUS DP Connection via PROFIBUS DP is a fast form of communication, however it can only be used to control the inputs and outputs of the S7-200. In order to communicate via PROFIBUS DP, you require the S7-200 communication module, the EM277. How to set up a connection to an S7-200 via PROFIBUS DP is described in detail in Entry ID 21915525." u dont need to use NCM , the configuration can be done with SIMATIC MANAGER with the same procedure this is a part of the article that dchartier also talked about and u can see it at: What are the options for accessing an S7-200 with WinCC? |
Last edited by: r.ethernet at: 8/3/2013 8:05 AMLast edited by: r.ethernet at: 8/3/2013 7:56 AM |
|
Follow us on