5/9/2012 5:40 PM | |
Posts: 557 Rating: (64) |
Hello, See attached setting. connect ethernet cable with same network. try browes option & try to get mac address. if you get both cp's mac address that means connections are ok. While communication(data transfer betweens 2 devices) 3 things are improtant. 1) protocal 2) connection 3) communication setting in both the devices. AttachmentCheck connection.pdf (167 Downloads) |
5/11/2012 10:03 AM | |
Posts: 10 Rating: (0) |
Hi Sie-enauto, Thank you for your advice. It would be very useful if I get your reference. Thanks in advance, Regards, CVS |
8/30/2013 1:39 PM | |
Joined: 4/21/2006 Last visit: 9/23/2024 Posts: 510 Rating: (24) |
New question was splitted to a new thread: connect 2 HMI ie OP177B with CPU? |
Follow us on