5/9/2012 1:05 PM | |
Posts: 10 Rating: (0) |
Dear Experts, I am new to this field. I am trying to communicate between two CPU 315-2DPs with cp 343-1 in the same project. I have tried with put and get funtions, I am not able to get connected. Igot no errors in netpro compiling. When i checked the instance db of get or put function blockI got error 0 status 19 or 1, it is blinking. I could not understand what would be the problem. I have searched this site and got some helpdocumentationon PUT/GET, basing on that I tried to implement for these cpus. But could not succeded. I also tried with send and rcv blocks also then i got error 1 and status 1. I have attached the trail project here. Anticipating your help.. Thanks in advance. Regards, CVS AttachmentPUT_GET.zip (216 Downloads) |
5/9/2012 1:12 PM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hello CVS, Have you seen this FAQ How do you program communication blocks FB14 "GET" and FB15 "PUT" for data exchange in the S7 program of an S7-300 CPU? Also How do you program communication blocks FB12 "BSEND" and FB13 "BRCV" for data exchange in the S7 program of an S7-300 CPU? CPU-CPU communication with SIMATIC controllers (compendium) |
Ammy |
|
5/9/2012 3:55 PM | |
Posts: 557 Rating: (64) |
Hello, in your program FB 200 PUT ID W#16#1. also you can try to change local id from netpro instead of 1 use 2. |
5/9/2012 4:07 PM | |
Posts: 10 Rating: (0) |
Hello Eastern, I did that, changing the Id 1 to 2.But no change.... Still it is same ... Error 0, status 25(dec). Thanks in advance Regards, Subha |
Follow us on