2/16/2015 1:41 PM | |
Joined: 4/14/2010 Last visit: 8/6/2024 Posts: 525 Rating: (11) |
Dear Sir, Many thanks for message, what about SIMATIC NET PC Software is this required in discussed option WinCC Web Server/Client and WinCC Server/Client for the configuration of CP1612 A2 and CP1623. is this included in WinCC 7.3 package for OS window 7 and what is the order code for that because there are several type of package regarding SIMATIC NET Software is this following..?? HARDNET-IE S7 = 6GK1716-1CB13-0AA0 SOFTNET-IE S7 = 6GK1704-1CW13-0AA0 What is the difference between WinCC User Archive 6AV6371-1CB07-3AX0 and WINCC/ARCHIVE V7.0, 1500 ARCHIVE TAGS 6AV6371-1DQ17-3AX0. what is the tag limit for WinCC User Archive 6AV6371-1CB07-3AX0 package...?? Regard's |
Last edited by: Sarfraz Bhatti at: 2/16/2015 2:11:57 PMMS |
|
2/19/2015 2:05 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2167)
|
Hello Muhammad Sarfraz, sorry, I am no expert in cables, this is part of Simatic Net. DCS has usually to do with PCS7 but maybe with WinCC inside the Simatic Manager too. See here https://support.industry.siemens.com/cs/ww/en/view/24023824 There is described a Minimalconfiguration. The point is here, to save a PC, by using a PC for Engineering-Station (ES) and Operating-Station (OS) at the "same" time.
Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
Follow us on