8/27/2016 1:59 PM | |
Joined: 5/1/2016 Last visit: 9/30/2024 Posts: 18 Rating: (0) |
Hello I have a machine with CPU 317 TF program Simatic S7-classic V5.5 and one with C-240 SIMOTION, scout program. I have the sofwares Scout V4.3 and S7-Technology V4.3. You can work on both machines with the same simatic-PG without installing virtual machines. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/29/2016 3:29:46 PMNew subject after splitting |
|
8/30/2016 7:31 AM | |
Joined: 5/12/2006 Last visit: 10/11/2024 Posts: 22410 Rating: (3017)
|
Hello, which Scout Version do you have exactly? Regards |
9/2/2016 7:35 AM | |
Joined: 5/12/2006 Last visit: 10/11/2024 Posts: 22410 Rating: (3017)
|
Hello, ok for the V3.2 of the S7317TF you need Scout V4.4, in V4.3 this device is not supported. The Scout V4.4 you can download here: https://support.industry.siemens.com/cs/ww/en/view/109480713 Regards |
This contribution was helpful to1 thankful Users |
9/12/2016 8:29 PM | |
Joined: 5/1/2016 Last visit: 9/30/2024 Posts: 18 Rating: (0) |
hello Christoph |
This contribution was helpful to1 thankful Users |
Follow us on