2/6/2018 6:32 PM | |
Posts: 2 Rating:
|
how can I parameterize a clock time and be able to see and edit it on the web page ... does not work ------------------------------------------------------------------------------------------ Attachmentpar.zip (293 Downloads) |
Last edited by: Jen_Moderator at: 2/7/2018 7:23:35 AMNew subject after splitting. Edited post for better reading. |
|
2/7/2018 8:51 AM | |
Posts: 2 Rating:
|
EVEN I AM CURIOUS THANKS |
2/7/2018 11:25 AM | |
Joined: 12/18/2014 Last visit: 9/12/2024 Posts: 33755 Rating:
|
Have now experimented further and have managed to visulise a complete cam for a weekly timer. For switching times, you have to take analog values and set them to Hex format. Then you can enter e.g. 9:00 am as number 900. Yesterday I also tried that and fell for a few nasty things and thought so, it does not work. The time is displayed 9:00 as 16 # 900. I wanted to change that in 10:00. Hurry up to the input: 16 # ... and oh, he denied the #. Then I enter the pure numeric value, 1000, press Return, and lo and behold, below the field is "submitted" but the field is empty. Then I gave up and chose the above path .. Today run again with analog value and Hex. I was then not irritated by the empty field and online in the LOGO! looked. And indeed, changed value has been entered. Go back to the web server and just click next to field ... suddenly the value will reappear. I'm sorry, but I have not seen any nonsense for a long time. In the appendix a screen video, my test file and the Web Editor test project. So that the curiosity has an end .... AttachmentWeb Editor Test.zip (466 Downloads) |
This contribution was helpful to
3 thankful Users |
Follow us on