11/4/2019 11:18 AM | |
Joined: 12/12/2016 Last visit: 7/25/2025 Posts: 640 Rating:
|
Hello, The Profinet Driver is not Open Source, so we cannot provide the sources. We updated the PNDriver to work with V2.4.0, it should be available on here (PN_Driver_IOT2000.zip) in the next days, with a new hash: 25dc9785aa580fac417a01ae168ec85f27a348e44c83858784d07b8697b5d6f3 If you need it urgently, please send me a pm with your Email and I can provide it to you. Kind regards! |
12/29/2019 11:30 PM | |
Joined: 2/16/2017 Last visit: 3/15/2024 Posts: 5 Rating:
|
FYI: the device driver sources I received (well, the GPL parts of it) can be found here: pndev-driver at sourcehut I fixed a minor issue and added a build manifest (as a buildroot package) so the sources can be tested in that regard. They still don't support kernels newer than 4.4, as far as I see (4.9 and above didn't work, IIRC). Porting work to current kernels shouldn't be hard but I don't have the capacities for it right now. Here's an example pndev driver build |
Follow us on