6/29/2022 10:46 AM | |
Joined: 1/21/2013 Last visit: 7/25/2024 Posts: 3019 Rating: (475) |
Hi lapgoch, maybe your issue is related to the used TLS version. As far as I remember, your PLC is not supporting TLS 1.2. When using Google Chrome (ore Microsoft Edge) you can try to use the Security panel inside the Chrome DevTools to figure out the security settings. Kind regards |
7/1/2022 9:11 AM | |
Joined: 1/21/2013 Last visit: 7/25/2024 Posts: 3019 Rating: (475) |
Hi lapgoch, then let's try it the different way. Please enable TLS 1.1 and also TLS 1.0 on Internet Options in your Windows operating system or when using Firefox in Firefox itself. The description from DigiCert should help you (even thought it for enabling TLS 1.1 and TLS 1.2). Kind regards |
7/1/2022 1:10 PM | |
Joined: 1/21/2013 Last visit: 7/25/2024 Posts: 3019 Rating: (475) |
Hi lapgoch, I searched for some information on the internet. It seems that in all modern browsers the support for TLS 1.0 and TLS 1.1 has been removed. Which - for security reasons - is a good fact. Since there is no possibility to enable TLS 1.2 on your PLC, you might have to use an older browser version. You can test the supported TLS version using the SSL/TLS Client Test from BrowserLeaks. Kind regards |
This contribution was helpful to1 thankful Users |
Follow us on