6/11/2021 11:24 AM | |
Joined: 2/27/2021 Last visit: 12/21/2022 Posts: 5 Rating: (0) |
I have enabled S7 access on both of the PLC, while Modbus access is unchecked. |
6/11/2021 12:56 PM | |
Joined: 12/18/2014 Last visit: 10/14/2024 Posts: 33954 Rating: (4221)
|
That's the reason because I only marked the S7 access. And work it now? |
6/16/2021 7:01 PM | |
Joined: 2/27/2021 Last visit: 12/21/2022 Posts: 5 Rating: (0) |
I can test it out in following days. So i need to allow both the S7 access and Modbus access? As is on picture 2.jpeg? |
6/16/2021 7:04 PM | |
Joined: 12/18/2014 Last visit: 10/14/2024 Posts: 33954 Rating: (4221)
|
You must only enable the Modbus access if you need a Modbus connection to Modbus devices. |
Follow us on