2/14/2012 9:41 AM | |
Joined: 1/9/2012 Last visit: 3/28/2024 Posts: 40 Rating: (5) |
In Modbus TCPthere arefour order types are available, 1] ModbusTCP CP- 2XV9 450-1MB00 2] ModbusTCP Red V1- 2XV9 450-1MB01 3] ModbusTCP Red V2- 2XV9 450-1MB11 4] ModbusTCP PN- 2XV9 450-1MB02 Currently i am working on ModbusTCP Red V1 (2XV9 450-1MB01). But to Test ModbusTCP Red V1, i am unable to get Library setup file (demo). I found a link which providesus manual for ModbusTCP Red V1. But the Library setup file (Demo) is not present here. Where as Libraries & Manualsfor types 1MB00,1MB11,1MB02are available at same link but for type 1MB01, there is no software/Library setup file available. Can anybody provide me any link where i can get the same? Thanks in advance. |
2/14/2012 11:28 AM | |
Joined: 10/3/2008 Last visit: 5/21/2024 Posts: 956 Rating: (123)
|
Hi, no other possibility, you have to wait... Wüstenräuber |
7/25/2013 2:42 PM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
New question was splitted to Open Modbus TCP redundant license for Redundant S7-412-5H CPU Best regards O_Moderator |
12/12/2016 9:24 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
New question published by CKO is split to a separate thread with the subject Manual of OPEN MODBUS/TCP RED. Best regards |