9/6/2014 4:04 PM | |
Joined: 9/27/2006 Last visit: 11/18/2024 Posts: 12296 Rating: (2691) |
Hello Sr. Oliveira; Have a look at ythe following docum,entation, it should give you enough information for your selection process: System Manual Modular Safety System (MSS) 3RK3 SIRIUS MSS DP Interface Module The DP interface is configured in the MSS system using the engineering tool "Modular Safety System ES". Matching configurations must be carried out in both engineering tools. Details on configuration can be found in the manual. The manual is available for download via the internet link stated below. Modular+Safety+System+ES+2008+SP4 - Siemens Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
9/8/2014 6:44 PM | |
Joined: 9/27/2006 Last visit: 11/18/2024 Posts: 12296 Rating: (2691) |
Hello Seu Oliveira; The first manual suggested shows in detailall the data exchanges that can be setup with a DP-master. A brief description can be found here: Delivery release: 3RK3 Modular Safety System The DP-Interface module serves the transmission of diagnostics and device state data to a superior PROFIBUS network. It supports the cyclic exchange of up to 32 bit with the control. Diagnostics data can be called up acyclically. For diagostics, you can read datasets using SFB52 or SFC59, seesection 8.4 "Diagnostics with Profibus". Look also at thie following FAQ: Hope this helps, Daniel Chartier |
Follow us on