5/13/2018 9:17 AM | |
Joined: 3/5/2015 Last visit: 1/2/2023 Posts: 32 Rating: (0) |
I am facing an issue here :( I have 400h redundant system. I am using only one CPU with two CP. I am using both the CP as Server Mosdbus and the second I am using as Client Modbus. The server is working fine. But the Client is not working. In the n/w connection it shows green but if i check the status i recieve an error A0FF. I checked the hw address called in OB1 and OB100. I checked the comm. Cycle time My CP is 443-1EX30-0XE0. The firmware version also seems to be fine.I have attached the program and the photos. Please help I went accross other siemens help page but still no solution I have attached the details related to my program in following link https://drive.google.com/open?id=1Z8eBvOF0VUo2lHpGQ-wj3PDvl7oP1Cr0 I am using the NW3 of OB1 and OB100 for the client config parameters calling. Then there is also one Modbus Nodes [ FC901] I am using. ------------------------------------------------------------------------------------------ |
Last edited by: Auto-max at: 5/13/2018 9:19:20 AMLast edited by: Jen_Moderator at: 5/14/2018 12:10:06 PMNew subject after splitting Last edited by: Auto-max at: 5/14/2018 3:50:09 PM |
|
5/18/2018 7:44 PM | |
Joined: 3/5/2015 Last visit: 1/2/2023 Posts: 32 Rating: (0) |
No help yet!! |
5/23/2018 8:47 AM | |
Joined: 6/19/2017 Last visit: 4/26/2024 Posts: 7952 Rating: (162) |
New question published by Auto-max is split to a separate thread with the subject When both our system communicate it is not working - A0FF error is coming . Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on