6/6/2009 8:32 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (306) |
Hello, I guess that you have a security issue. The NC wants to access to the folder in the PC over the network, butI am afraid that the NC is not a known user in the PC. Look to the security properties of the folder. Like explained here: http://www.microsoft.com/windowsxp/using/security/learnmore/accesscontrol.mspx or here http://support.microsoft.com/kb/308419 Settings depends on following points: - is the computer in a domain or a workgroup - is simplified or advanced sharing activated I am not sure, but may be you have to activate the user "guest" andadd the user "guest" to the accounts allowed to access the folder. Pay attention that doing that gives acces to the folder by anyone. |
Best regards |
|
6/9/2009 5:21 AM | |
Joined: 3/3/2008 Last visit: 10/5/2023 Posts: 333 Rating: (51) |
hi i would like to know whether the you have created a rcs login and using that login have youalready logged. if you are logged, whether you are able to ping between the PC and th 802DSL -PCU. iam just attaching a procedure for the RCS execution regards Ram AttachmentInstructions for execution a part program from external via Ethernet.pdf (345 Downloads) |
Follow us on