3/20/2023 11:25 AM | |
Joined: 5/24/2016 Last visit: 9/13/2024 Posts: 347 Rating: (52)
|
In that case I would like to present to you a 3rd option. 7 Axis on the 828D PPU is to much as a stand alone, as you say you need a NX modul. Now my 3d option is to make the magazine a standalone unit using a S120 AC/AC system. Reason for this is that this system is mechanically already a stand alone system that does not need to work with high degree of accuracy with other axis. Where as the spindle might have to work in a synchronized manner with the Z axis in for example Tap threadning. I have made a quick sizer project in Sizer 3.19 of this. Now of course cable lenghts, motor sizes and so on is not correct, but is just for reference. for your 2nd option using the G120 for the spindle. It should be possible, and I would think you should be able to connect the last SMC for the feedback to X102 on the PPU and set the topology accordingly an using the X252 terminal on the PPU as the analog set point, but it would not recommed it, and it is not a solution that is possible to setup on Sizer (I tried) so I can not verify it. Best Regards Riddersholm Attachment828D - 7Axis S120 - Magazine Standalone - Pfuser .zip (315 Downloads) |
Follow us on