11/8/2020 5:44 AM | |
Joined: 12/18/2014 Last visit: 8/7/2024 Posts: 33500 Rating: (4162)
|
Hello Meshell57, at first welcome to the Forum. The "Access Control" function is only available for LOGO! 0BA8 base modules. AttachmentLOGO! 8 manual 0BA8 2014_06 page 4.pdf (178 Downloads) |
Last edited by: ixo65 at: 11/08/2020 05:44:51 |
|
11/8/2020 9:52 AM | |
Joined: 12/18/2014 Last visit: 8/7/2024 Posts: 33500 Rating: (4162)
|
I still have a description of the old LOGO! App from 2013 found. There was no 0BA8 yet. And as you can see there, there is nothing to be read about access control and web server. Maybe it is enough if you are using the current version of the LOGO! App only select 0BA7 instead of 0BA8.
AttachmentLOGO! App V1.0.0 english 08_2013.pdf (184 Downloads) |
11/8/2020 10:00 AM | |
Joined: 11/8/2020 Last visit: 6/13/2024 Posts: 5 Rating: (0) |
thank you , this is helpfull. When i get everything up and running (again) i will post my findings here! |
Follow us on