1/23/2019 4:30 PM | |
Joined: 8/18/2015 Last visit: 11/24/2023 Posts: 8 Rating:
|
As you know, S7-GRAPH is not available for the S7-1200. All those who miss this should have a look at the software Grafcet-Studio. This allows you to program an S7-1200 with Grafcet DIN EN 60848. Grafcet-Studio can then be used to create sequences of steps and download them to the S7-1200 PLC. In order for this to work, the TIA portal must download some blocks (Grafcet engine) into the S7-1200. The Grafcet-Studio software can now program the S7-1200 without the TIA PORTAL. For all who are interested in this matter, here is the link to the description: In addition, Grafcet-Studio can also be used in the same way for the following devices:
A demo version can be requested here free of charge: https://www.mhj-online.de/request-a-demo Best regards |
This contribution was helpful to
2 thankful Users |
Follow us on