2/23/2022 8:54 AM | |
Joined: 2/17/2020 Last visit: 5/3/2024 Posts: 995 Rating: (170) |
Hi, Following the compatibility list of WinCC V7.4, you could use the following released Virus scanners: - McAfee Application Control: V7.0 or V6.2.0 (not approved in combination with Windows 10). - McAfee Endpoint Protection Suite: V10.2 or V8.8 - McAfee VirusScan Enterprise: V8.8 -Microsoft Defender Antivirus: version of installed operation system - Symantec Endpoint Protection: V12.1.6, V12.1.5 or V12.1. - Trend MICRO OfficeScan (for WinCC only the "Corporate Edition" of the Trend Micro OfficeScan virus scanner is approved): V11.0 SP1 or V11.0. - Trend MICRO OfficeScan Client-Server Suite: V11.0. Any antivirus that does not comply with the above would put the correct operation of WinCC V7.4 at risk. AttachmentWinCC_V7.4_compatibility-list_en_2021-12-23.zip (170 Downloads) |
A rating will be well appreciated. |
|
Follow us on