1/10/2024 5:52 PM | |
Joined: 8/17/2022 Last visit: 1/10/2024 Posts: 6 Rating: (0) |
I am currently using the newly released version of LWE 1.2 When launching a project to AWS and choosing to create a new environment, the newborn environment uses a nondeprecated Tomcat platform, which seems to be incompatible with the project. This is the message it returns: "Application's Java version is lower than the environment's" And there you have a non-functional dashboard... If I downgrade the environment to an earlier but deprecated platform, it all goes well. The problem is that this platform is doomed to become inoperative on certain unannounced dates. I fear that all my customer's dashboards are doomed as well. What´s the turnaround for this? Are there new policies or rules that need to be included? Regards, Artur ------------------------------------------------------------------------------------------ |
Last edited by: ArturSentinel at: 01/10/2024 17:54:24Last edited by: Jen_Moderator at: 01/11/2024 12:02:36New subject after splitting |
|
1/15/2024 10:02 AM | |
Joined: 9/19/2018 Last visit: 8/6/2024 Posts: 386 Rating: (46)
|
We recommend using JavaCorretto 11 for LWE 1.2, details see attached Word file. AttachmentAccess to web app failure after deploy LWE V1.2 project to AWS.docx (247 Downloads) |
Follow us on