12/20/2013 10:18 AM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (40) |
..... I'm sure it is possible to then set all the properties of this window but i do not know where to start. <-- This information would be golden!! I would like to remove the titlebar, and remove the option to close the window. Also, multiple clicks of the button opens multiple windows. I only need one window. ... Hi bradders, it schould be possible to change this settings inside the os-project editor. Regards, Healthcheck |
Last edited by: Healthcheck at: 12/20/2013 10:19 AMGrundkurs/Systemkurs WinCC V7: |
|
Follow us on