3/10/2016 1:20 PM | |
Joined: 9/23/2005 Last visit: 11/15/2024 Posts: 4793 Rating: (733) |
Is this what you are looking for? |
Regards, |
|
3/10/2016 1:34 PM | |
Joined: 6/13/2010 Last visit: 11/8/2024 Posts: 35 Rating: (0) |
yes, i allready have this and i'm more cofiused |
3/11/2016 1:30 PM | |
Joined: 6/13/2010 Last visit: 11/8/2024 Posts: 35 Rating: (0) |
hello, after several atempts some things are clear and some not, I have attached the screens question! i can't understand the reference point of leading axis and the leading axis point in relation of the cam table value. #can i start a cam from the midle point of a cam table. in my aplication two difrent cams are working togather after several cycles i noticed that the cams have moved from the original point i use non cyclic cams due the large format length 80m long and the cams are in the end-start point Attachmentcam.pdf (222 Downloads) |
Last edited by: misak_s at: 3/11/2016 1:35:46 PMLast edited by: misak_s at: 3/11/2016 1:37:06 PM |
|
Follow us on